ACTION#.SOURCETEXT

Description

This parameter defines the text associated with an ACTION Source.

To clear the text stored, use issue: ACTION#.SOURCETEXT clear to remove the text and commands.

Action Sources Using SOURCETEXT:

Versions

Action Version Notes
Implemented 02-05-01-000

General Information

Type

Read/Write

Units

N/A

Range

N/A

Default Value

 

Data Type

String

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported